Overview

Wi-SUN is a wireless communication standard aiming to enable large-scale IOT networks in a mesh structure. The network typically consists of line powered routers and gateways, and battery powered end nodes. The Wi-SUN FAN Specification is given by the Wi-SUN Alliance.

In TI Wi-SUN FAN Stack, the 6LoWPAN, RPL, IPv6, ICMPv6 and UDP layers have been adapted from open source components. An overview of the SW components is given in Figure 20.

../_images/block-diagram.png

Figure 20. TI Wi-SUN FAN Stack Overview

What is a FAN?

FAN - field area network is a network type aiming for connectivity on a larger scale. Example uses are within a smart city. To achieve this, the FAN consists of multiple smaller personal area networks (PANs). The FAN can connect to a Wide area network (WAN) in order to grow the scale even more.

Within each PAN, nodes assume one of three operational roles (set via the local administrative policy):

  • Each PAN contains a Border Router providing WAN connectivity to the PAN. The Border Router maintains source routing tables for all nodes within its PAN, provides node authentication and key management services, and disseminates PAN wide information such as broadcast schedules.

  • Router node, which provides upward and downward packet forwarding (within a PAN). A Router also provides services for relaying security and address management protocols.

  • Leaf nodes provide minimum capabilities: discovering and joining a PAN, send/receive IPv6 packets, etc. (Leaf node role is not implemented in TI Wi-SUN FAN.)

The node roles and network leves are visualized in Figure 21.

../_images/nw_topology_wisun.png

Figure 21. FAN Overview

Architecture Choices

TI Wi-SUN FAN Stack can be used in two separate architectures based on the end product application. Figure 22. shows the two different system architectures enabled by TI Wi-SUN FAN Stack.

../_images/fig-device-configuration.png

Figure 22. NWP and Embedded Configurations

  • A co-processor is shown in Figure 22. (left). The protocol stack runs on the device while the application is executed on an external MPU or MCU. The application interfaces with the device using the network protocol interface (NWP) over a serial universal asynchronous receiver/transmitter (UART) connection. This configuration is useful for cases where the application image is large. If the application is run from a host device, it will not be limited by the flash size of the device. The NWP interface is documented in the TI Wi-SUN FAN NWP Interface Guide.

  • A single device is shown in Figure 22. (right). The application and protocol stack are both implemented on the embedded device as a true single-chip solution.This configuration is the simplest and most common for network nodes.

Please see the Example Application Guide for availability of the modes on specific part numbers.

Network Profiles

The TI Wi-SUN FAN Stack supports three network profiles to optimize network performance that can be selected in SysConfig -> TI Wi-SUN FAN -> Advanced.

  1. Maximize responsiveness

  2. Balanced mode

  3. Maximize scalability

When selecting a network profile the internal network timing and behavior is adjusted to meet the requirements of the network size. The following settings are set to the recommended value for the selected network profile in SysConfig.

  • Rapid join: Calibrated settings for an expedited join process are used for Maximize responsiveness networks.

  • MPL low latency: Latency optimizations for multicast forwarding. Since this feature is not Wi-SUN compliant, it is not used by default in all three network profiles.

  • Disconnection detection times: The time it takes for a Router Node (RN) to recognize a disconnection from the Border Router (BR) and vice versa. Appropriate values for disconnection detection times are used based on the selected network profile. These values directly affect trade off between responsiveness vs scalability.

The modification of these settings is possible but not recommended and could result in reduced performance.

We recommend starting by using the Maximize responsiveness profile. This profile configures the network for rapid join time, rapid disconnection detection, rapid PAN timeout and rapid DIO updates. If you experience data overflow, we recommend switching to the Balanced mode profile which will allow longer timeouts for the initial key transmission and increases the disconnection detection time, the PAN timeout and the DIO message intervals. If you expand your network to the point where you need to further minimize data overflow, you can switch to the Maximize scalability profile which will configure even longer intervals to further reduce network traffic and allow slower responses.