![]() |
![]() |
|
TI BLE5-Stack API Documentation
2.2.11.00
|
Macros | |
| #define | RTLSSRV_BAD_PARAMETER 0x12 |
| Invalid parameter. | |
| #define | RTLSSRV_COMMAND_DISALLOWED 0x0C |
| Disallowed Command. | |
| #define | RTLSSRV_CONN_HANDLE_INVALID 0x02 |
| Invalid Handle. | |
| #define | RTLSSRV_ERROR_DUE_TO_LIMITED_RESOURCES 0x0D |
| Limited Resources. | |
| #define | RTLSSRV_FEATURE_NOT_SUPPORTED 0x11 |
| Unsupported Feature. | |
| #define | RTLSSRV_OUT_OF_MEMORY 0x07 |
| Out of Memory. | |
| #define | RTLSSRV_REMOTE_FEATURE_NOT_SUPPORTED 0x1A |
| Unsupported Remote Feature. | |
| #define | RTLSSRV_UNKNOWN_ADVERTISING_IDENTIFIER 0x42 |
| Unknown Advertising Identifier. | |
Error codes used to parse RTLSSRV_ERROR_EVT Errors produced by HCI are mapped to their respective HCI Error values