TI BLE5-Stack API Documentation  2.2.11.00
Data Fields
extImgEnableReq_t Struct Reference

Data Fields

uint8_t cmdID
 Ext Ctrl Op-code.
 
uint8_t imgNo
 Image Number.
 
uint8_t imgType
 Image Type.
 
uint16_t techType
 Wireless technology type.
 

Detailed Description

The extended payload of an OAD_EXT_CTRL_ENABLE_IMG command

Note
This is the extended version of the command, there is a short version with just the op-code that will enable the last downloaded image.

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale