TI-15.4 Stack API
Data Fields
_apimac_securitypibkeydeviceentry Struct Reference

#include <api_mac.h>

Collaboration diagram for _apimac_securitypibkeydeviceentry:
Collaboration graph
[legend]

Data Fields

uint16_t keyIndex
 
uint16_t keyDeviceIndex
 
ApiMac_keyDeviceDescriptor_t deviceEntry
 

Detailed Description

Security PIB Key ID device entry for a Get/Set ApiMac_securityAttribute_keyDeviceEntry

Field Documentation

§ keyIndex

uint16_t _apimac_securitypibkeydeviceentry::keyIndex

index into the macKeyDeviceList

§ keyDeviceIndex

uint16_t _apimac_securitypibkeydeviceentry::keyDeviceIndex

index into macKeyDeviceList[keyIndex]

§ deviceEntry

ApiMac_keyDeviceDescriptor_t _apimac_securitypibkeydeviceentry::deviceEntry

Place to put the requested data


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale