TI-15.4 Stack API
Data Fields
_apimac_securitypibkeyentry Struct Reference

#include <api_mac.h>

Data Fields

uint16_t keyIndex
 
uint8_t keyEntry [APIMAC_KEY_MAX_LEN]
 
uint32_t frameCounter
 

Detailed Description

Security PIB Key entry for a Get/Set ApiMac_securityAttribute_keyEntry

Field Documentation

§ keyIndex

uint16_t _apimac_securitypibkeyentry::keyIndex

index into the macKeyTable

§ keyEntry

uint8_t _apimac_securitypibkeyentry::keyEntry[APIMAC_KEY_MAX_LEN]

key entry

§ frameCounter

uint32_t _apimac_securitypibkeyentry::frameCounter

frame counter


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale