TI BLE-Stack for Bluetooth API Documentation  3.03.00.00
Data Fields
gapEstLinkReq_t Struct Reference

Establish Link Request parameters. More...

Data Fields

uint8 addrTypePeer
 Address type of the advertiser: Address Types.
 
uint8 highDutyCycle
 TRUE to high duty cycle scan, FALSE if not.
 
uint8 peerAddr [B_ADDR_LEN]
 Advertiser's address.
 
uint8 taskID
 Requesting App/Profile's Task ID.
 
uint8 whiteList
 Determines use of the white list: GAP White List Options.
 

Detailed Description

Establish Link Request parameters.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale