![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
GATT Structure for Characteristic Presentation Format Value. More...
Data Fields | |
uint16 | desc |
Description of this attribute as defined in a higher layer profile. | |
int8 | exponent |
A sign integer which represents the exponent of an integer. | |
uint8 | format |
Format of the value of this characteristic. | |
uint8 | nameSpace |
Name space of the description. | |
uint16 | unit |
Unit of this attribute as defined in the data dictionary. | |
GATT Structure for Characteristic Presentation Format Value.