![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.00.00
|
Parameter Structure for Response to SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_RSP. More...
Data Fields | |
uint16_t | attrHandle |
2 Byte attribute handle of the characteristic value. | |
uint8_t | status |
1 Byte status of the request (SUCCESS or Error, List of SNP error codes) | |
Parameter Structure for Response to SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_RSP.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.