![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.03.00
|
LinkDB layer interface.
Go to the source code of this file.
Data Structures | |
struct | encParams_t |
Encryption Params. More... | |
struct | linkDBInfo_t |
linkDB info More... | |
struct | linkDBItem_t |
linkDB item More... | |
struct | linkSec_t |
SRK and Sign Counter. More... | |
Macros | |
#define | INVALID_CONNHANDLE 0xFFFF |
Invalid connection handle, used for no connection handle. | |
#define | LINBDB_ERR_INSUFFICIENT_KEYSIZE 0x0c |
Link is encrypted but the key size is too small. | |
#define | LINK_AUTHENTICATED 0x02 |
Link is authenticated. | |
#define | LINK_BOUND 0x04 |
Link is bonded. | |
#define | LINK_CONNECTED 0x01 |
Link is connected. | |
#define | LINK_ENCRYPTED 0x10 |
Link is encrypted. | |
#define | LINK_IN_UPDATE 0x40 |
Link is in update procedure. | |
#define | LINK_NOT_CONNECTED 0x00 |
Link isn't connected. | |
#define | LINK_SECURE_CONNECTIONS 0x20 |
Link uses Secure Connections. | |
#define | linkDB_Authenticated(connectionHandle) linkDB_State( (connectionHandle), LINK_AUTHENTICATED ) |
Check to see if the physical link is authenticated. More... | |
#define | linkDB_Bonded(connectionHandle) linkDB_State( (connectionHandle), LINK_BOUND ) |
Check to see if the physical link is bonded. More... | |
#define | LINKDB_CONNHANDLE_ALL LL_CONNHANDLE_ALL |
Terminates all links. | |
#define | LINKDB_CONNHANDLE_INVALID LL_CONNHANDLE_INVALID |
Invalid connection handle, used for no connection handle. | |
#define | LINKDB_CONNHANDLE_LOOPBACK LL_CONNHANDLE_LOOPBACK |
Loopback connection handle, used to loopback a message. | |
#define | linkDB_Encrypted(connectionHandle) linkDB_State( (connectionHandle), LINK_ENCRYPTED ) |
Check to see if the physical link is encrypted. More... | |
#define | LINKDB_ERR_INSUFFICIENT_AUTHEN 0x05 |
Link isn't even encrypted. | |
#define | LINKDB_ERR_INSUFFICIENT_ENCRYPTION 0x0f |
Link is encrypted but it's not authenticated. | |
#define | LINKDB_STATUS_UPDATE_NEW 0 |
New connection created. | |
#define | LINKDB_STATUS_UPDATE_REMOVED 1 |
Connection was removed. | |
#define | LINKDB_STATUS_UPDATE_STATEFLAGS 2 |
Connection state flag changed. | |
#define | linkDB_Up(connectionHandle) linkDB_State( (connectionHandle), LINK_CONNECTED ) |
Check to see if a physical link is up (connected). More... | |
#define | LOOPBACK_CONNHANDLE 0xFFFE |
Loopback connection handle, used to loopback a message. | |
Typedefs | |
typedef void(* | pfnLinkDBCB_t) (uint16 connectionHandle, uint8 changeType) |
function pointer used to register for a status callback | |
typedef void(* | pfnPerformFuncCB_t) (linkDBItem_t *pLinkItem) |
function pointer used to perform specialized link database searches | |
Functions | |
uint8 | linkDB_Add (uint8 taskID, uint16 connectionHandle, uint8 stateFlags, uint8 addrType, uint8 *pAddr, uint8 *pAddrPriv, uint8 connRole, uint16 connInterval, uint16 MTU) |
Adds a record to the link database. More... | |
uint8 | linkDB_Authen (uint16 connectionHandle, uint8 keySize, uint8 mitmRequired) |
Check to see if the physical link is encrypted and authenticated. More... | |
linkDBItem_t * | linkDB_Find (uint16 connectionHandle) |
Find the link. More... | |
linkDBItem_t * | linkDB_FindFirst (uint8 taskID) |
Find the first link that matches the taskID. More... | |
uint8 | linkDB_GetInfo (uint16 connectionHandle, linkDBInfo_t *pInfo) |
Get information about a link. More... | |
NODOC void | linkDB_Init (void) |
Initialize the Link Database. | |
uint16 | linkDB_MTU (uint16 connectionHandle) |
This function is used to get the MTU size of a link. More... | |
uint8 | linkDB_NumActive (void) |
Return the number of active connections. More... | |
uint8 | linkDB_NumConns (void) |
return the maximum number of connections supported. More... | |
void | linkDB_PerformFunc (pfnPerformFuncCB_t cb) |
Perform a function of each connection in the link database. More... | |
uint8 | linkDB_Register (pfnLinkDBCB_t pFunc) |
Register with linkDB. More... | |
uint8 | linkDB_Remove (uint16 connectionHandle) |
Remove a record from the link database. More... | |
uint8 | linkDB_Role (uint16 connectionHandle) |
Get the role of a physical link. More... | |
void | linkDB_SecurityModeSCOnly (uint8 state) |
Set a device into Secure Connection Only Mode. More... | |
uint8 | linkDB_State (uint16 connectionHandle, uint8 state) |
Check to see if a physical link is in a specific state. More... | |
uint8 | linkDB_Update (uint16 connectionHandle, uint8 newState, uint8 add) |
Update the stateFlags of a link record. More... | |
uint8 | linkDB_UpdateMTU (uint16 connectionHandle, uint16 newMtu) |
update the MTU size of a link or record. More... | |