TI BLE5-Stack API Documentation  1.01.10.00
Data Fields
GapAdv_scanReqReceived_t Struct Reference

Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event. More...

Data Fields

uint8 channel
 Channel when the scan req was received.
 
uint8 handle
 Advertising handle.
 
int8 rssi
 RSSI of the scan req.
 
uint8 scanAddr [B_ADDR_LEN]
 Address of scanning device.
 
uint8 scanAddrType
 Address type of scanning device.
 

Detailed Description

Data type returned with GAP_EVT_SCAN_REQ_RECEIVED event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale