TI BLE5-Stack API Documentation  1.01.10.00
Data Fields
attReadMultiReq_t Struct Reference

Read Multiple Request format. More...

Data Fields

uint16 numHandles
 Number of attribute handles.
 
uint8 * pHandles
 Set of two or more attribute handles (4 to ATT_MTU_SIZE-1) - must be first field.
 

Detailed Description

Read Multiple Request format.

for method ATT_READ_MULTI_REQ


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale