TI BLE5-Stack API Documentation  1.01.12.00
Data Fields
gapPeriConnectParams_t Struct Reference

Data Fields

uint16_t intervalMax
 Maximum value for the connection event (interval. 0x0006 - 0x0C80 * 1.25 ms)
 
uint16_t intervalMin
 Minimum value for the connection event (interval. 0x0006 - 0x0C80 * 1.25 ms)
 
uint16_t latency
 Number of LL latency connection events (0x0000 - 0x03e8)
 
uint16_t timeout
 Connection Timeout (0x000A - 0x0C80 * 10 ms)
 

Detailed Description

Peripheral Preferred Connection Parameters.

This is used to set the GGS_PERI_CONN_PARAM_ATT param with GGS_SetParameter


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale