TI BLE5-Stack API Documentation  1.01.12.00
Data Fields
gapUpdateLinkParamReq_t Struct Reference

Data Fields

uint16_t connectionHandle
 Connection handle of the update.
 
uint16_t connLatency
 Connection Latency.
 
uint16_t connTimeout
 Connection Timeout.
 
uint16_t intervalMax
 Maximum Connection Interval.
 
uint16_t intervalMin
 Minimum Connection Interval.
 
uint8_t signalIdentifier
 L2CAP Signal Identifier. Must be 0 for LL Update.
 

Detailed Description

Establish Link Request parameters

This is used by GAP_UpdateLinkParamReq


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale