TI BLE5-Stack API Documentation  1.01.12.00
Data Fields
hciEvt_BLEReadRemoteFeatureComplete_t Struct Reference

LE Read Remote Used Features Complete Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connectionHandle
 connection handle
 
uint8 features [8]
 features
 
osal_event_hdr_t hdr
 osal event header
 
uint8 status
 status of event
 

Detailed Description

LE Read Remote Used Features Complete Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale