Struct containing the parameters required for verifying a message. More...
#include <ECDSA.h>
Data Fields | |
const ECCParams_CurveParams * | curve |
const CryptoKey * | theirPublicKey |
const uint8_t * | hash |
const uint8_t * | r |
const uint8_t * | s |
Struct containing the parameters required for verifying a message.
const ECCParams_CurveParams* ECDSA_OperationVerify::curve |
A pointer to the elliptic curve parameters
const CryptoKey* ECDSA_OperationVerify::theirPublicKey |
A pointer to the public key of the party that signed the hash of the message
const uint8_t* ECDSA_OperationVerify::hash |
A pointer to the hash of the message. Must be the same length as the other curve parameters.
const uint8_t* ECDSA_OperationVerify::r |
A pointer to the r component of the received signature. Must be of the same length as other params of the curve used.
const uint8_t* ECDSA_OperationVerify::s |
A pointer to the s component of the received signature. Must be of the same length as other params of the curve used.