RF scheduler policy. More...
#include <RF.h>
Data Fields | |
RF_SubmitHook | submitHook |
Function hook implements the scheduling policy to be executed at the time of RF_scheduleCmd API call. More... | |
RF_ConflictHook | conflictHook |
Function hook implements the runtime conflict resolution, if any identified at the start time of next command. More... | |
RF scheduler policy.
This data structure contains function hooks which implements the scheduling algorithm used to inter-align one or more independent protocol stacks.
RF_SubmitHook RFCC26XX_SchedulerPolicy::submitHook |
Function hook implements the scheduling policy to be executed at the time of RF_scheduleCmd API call.
RF_ConflictHook RFCC26XX_SchedulerPolicy::conflictHook |
Function hook implements the runtime conflict resolution, if any identified at the start time of next command.