SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_SlCmdExt_t Struct Reference

Data Fields

_u16 TxPayload1Len
 
_u16 TxPayload2Len
 
_i16 RxPayloadLen
 
_i16 ActualRxPayloadLen
 
_u8 * pTxPayload1
 
_u8 * pTxPayload2
 
_u8 * pRxPayload
 

Detailed Description

Definition at line 217 of file driver.h.

Field Documentation

§ ActualRxPayloadLen

_i16 ActualRxPayloadLen

Definition at line 222 of file driver.h.

§ pRxPayload

_u8* pRxPayload

Definition at line 225 of file driver.h.

§ pTxPayload1

_u8* pTxPayload1

Definition at line 223 of file driver.h.

§ pTxPayload2

_u8* pTxPayload2

Definition at line 224 of file driver.h.

§ RxPayloadLen

_i16 RxPayloadLen

Definition at line 221 of file driver.h.

§ TxPayload1Len

_u16 TxPayload1Len

Definition at line 219 of file driver.h.

§ TxPayload2Len

_u16 TxPayload2Len

Definition at line 220 of file driver.h.


The documentation for this struct was generated from the following file: