SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_SlProtocolNetAppReceiveRequest_t Struct Reference

Data Fields

_u16 Handle
 
_u16 MaxBufferLen
 
_u32 Flags
 

Detailed Description

Definition at line 1016 of file protocol.h.

Field Documentation

§ Flags

_u32 Flags

Definition at line 1020 of file protocol.h.

§ Handle

_u16 Handle

Definition at line 1018 of file protocol.h.

§ MaxBufferLen

_u16 MaxBufferLen

Definition at line 1019 of file protocol.h.


The documentation for this struct was generated from the following file: