SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlDeviceVersionReadResponsePart_t Struct Reference

Data Fields

_u32 ChipId
 
_u32 FwVersion [4]
 
_u8 PhyVersion [4]
 

Detailed Description

Definition at line 490 of file protocol.h.

Field Documentation

§ ChipId

_u32 ChipId

Definition at line 492 of file protocol.h.

§ FwVersion

_u32 FwVersion[4]

Definition at line 493 of file protocol.h.

§ PhyVersion

_u8 PhyVersion[4]

Definition at line 494 of file protocol.h.


The documentation for this struct was generated from the following file: