SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlFsProgramCommand_t Struct Reference

Data Fields

_u16 KeyLen
 
_u16 ChunkLen
 
_u32 Flags
 

Detailed Description

Definition at line 1257 of file protocol.h.

Field Documentation

§ ChunkLen

_u16 ChunkLen

Definition at line 1260 of file protocol.h.

§ Flags

_u32 Flags

Definition at line 1261 of file protocol.h.

§ KeyLen

_u16 KeyLen

Definition at line 1259 of file protocol.h.


The documentation for this struct was generated from the following file: