SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlSocketAddrIPv6EUI48Command_t Struct Reference

Data Fields

_i16 LenOrPadding
 
_u8 Sd
 
_u8 FamilyAndFlags
 
_u16 Port
 
_u8 Address [6]
 

Detailed Description

Definition at line 834 of file protocol.h.

Field Documentation

§ Address

_u8 Address[6]

Definition at line 840 of file protocol.h.

§ FamilyAndFlags

_u8 FamilyAndFlags

Definition at line 838 of file protocol.h.

§ LenOrPadding

_i16 LenOrPadding

Definition at line 836 of file protocol.h.

§ Port

_u16 Port

Definition at line 839 of file protocol.h.

§ Sd

_u8 Sd

Definition at line 837 of file protocol.h.


The documentation for this struct was generated from the following file: