SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlWlanConnectCommon_t Struct Reference

Data Fields

_u8 SecType
 
_u8 SsidLen
 
_u8 Bssid [6]
 
_u8 PasswordLen
 

Detailed Description

Definition at line 540 of file protocol.h.

Field Documentation

§ Bssid

_u8 Bssid[6]

Definition at line 543 of file protocol.h.

§ PasswordLen

_u8 PasswordLen

Definition at line 544 of file protocol.h.

§ SecType

_u8 SecType

Definition at line 541 of file protocol.h.

§ SsidLen

_u8 SsidLen

Definition at line 542 of file protocol.h.


The documentation for this struct was generated from the following file: