SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlWlanGetNetworkListCommand_t Struct Reference

Data Fields

_u8 Index
 
_u8 Count
 
_i8 padding [2]
 

Detailed Description

Definition at line 641 of file protocol.h.

Field Documentation

§ Count

_u8 Count

Definition at line 644 of file protocol.h.

§ Index

_u8 Index

Definition at line 643 of file protocol.h.

§ padding

_i8 padding[2]

Definition at line 645 of file protocol.h.


The documentation for this struct was generated from the following file: