SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlWlanSmartConfigParams_t Struct Reference

Data Fields

_u32 GroupIdBitmask
 
_u8 Cipher
 
_u8 PublicKeyLen
 
_u8 Padding [2]
 

Detailed Description

Definition at line 657 of file protocol.h.

Field Documentation

§ Cipher

_u8 Cipher

Definition at line 660 of file protocol.h.

§ GroupIdBitmask

_u32 GroupIdBitmask

Definition at line 659 of file protocol.h.

§ Padding

_u8 Padding[2]

Definition at line 662 of file protocol.h.

§ PublicKeyLen

_u8 PublicKeyLen

Definition at line 661 of file protocol.h.


The documentation for this struct was generated from the following file: