SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlSocketAddrResponse_u Union Reference

Data Fields

SlSocketAddrAsyncIPv4Response_t IpV4
 
SlSocketAddrAsyncIPv6EUI48Response_t IpV6EUI48
 
SlSocketAddrAsyncIPv6Response_t IpV6
 

Detailed Description

Definition at line 861 of file protocol.h.

Field Documentation

§ IpV4

Definition at line 862 of file protocol.h.

§ IpV6

Definition at line 865 of file protocol.h.

§ IpV6EUI48

Definition at line 863 of file protocol.h.


The documentation for this union was generated from the following file: