RAM implementation of the NVS driver.
============================================================================
This NVS driver implementation makes use of RAM instead of FLASH memory. It can be used for developing code which relies the NVS driver without wearing down FLASH memory.
The NVS header file should be included in an application as follows:
#include <stdint.h>
#include <stdbool.h>
Go to the source code of this file.
Data Structures | |
struct | NVSRAM_HWAttrs |
NVSRAM Hardware Attributes. More... | |
struct | NVSRAM_Object |
Variables | |
const NVS_FxnTable | NVSRAM_fxnTable |
const NVS_FxnTable NVSRAM_fxnTable |