![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.02.04.00
|
Macros | |
| #define | GAP_EVT_ADV_DATA_TRUNCATED (uint32_t)BV(6) |
| #define | GAP_EVT_ADV_END (uint32_t)BV(3) |
| #define | GAP_EVT_ADV_END_AFTER_DISABLE (uint32_t)BV(1) |
| #define | GAP_EVT_ADV_EVT_MASK |
| Mask for all advertising events. More... | |
| #define | GAP_EVT_ADV_REPORT (uint32_t)BV(22) |
| #define | GAP_EVT_ADV_REPORT_FULL (uint32_t)BV(23) |
| #define | GAP_EVT_ADV_SET_TERMINATED (uint32_t)BV(4) |
| #define | GAP_EVT_ADV_START (uint32_t)BV(2) |
| #define | GAP_EVT_ADV_START_AFTER_ENABLE (uint32_t)BV(0) |
| #define | GAP_EVT_INSUFFICIENT_MEMORY (uint32_t)BV(31) |
| A memory failure has occurred. | |
| #define | GAP_EVT_SCAN_DISABLED (uint32_t)BV(17) |
| #define | GAP_EVT_SCAN_DUR_ENDED (uint32_t)BV(19) |
| Scan duration has ended. | |
| #define | GAP_EVT_SCAN_ENABLED (uint32_t)BV(16) |
| Scanner has been enabled. | |
| #define | GAP_EVT_SCAN_EVT_MASK |
| Mask for all scan events. More... | |
| #define | GAP_EVT_SCAN_INT_ENDED (uint32_t)BV(20) |
| #define | GAP_EVT_SCAN_PRD_ENDED (uint32_t)BV(18) |
| #define | GAP_EVT_SCAN_REQ_RECEIVED (uint32_t)BV(5) |
| #define | GAP_EVT_SCAN_WND_ENDED (uint32_t)BV(21) |
| Scan window has ended. | |
These are received through the pfnGapCB_t registered in the GapAdv_create
See the individual event to see how pBuf in the pfnGapCB_t should be cast.
| #define GAP_EVT_ADV_DATA_TRUNCATED (uint32_t)BV(6) |
Sent when the advertising data is truncated due to the limited advertisement data length for connectable advertisements.
pBuf should be cast to GapAdv_truncData_t
| #define GAP_EVT_ADV_END (uint32_t)BV(3) |
Sent after each advertisement (for legacy advertising) or at the end of each each advertisement set (for extended advertising)
pBuf should be cast to a uint8_t which will contain the advertising handle
| #define GAP_EVT_ADV_END_AFTER_DISABLE (uint32_t)BV(1) |
Sent after advertising stops due to a GapAdv_disable
pBuf should be cast to a uint8_t which will contain the advertising handle
| #define GAP_EVT_ADV_EVT_MASK |
Mask for all advertising events.
| #define GAP_EVT_ADV_REPORT (uint32_t)BV(22) |
An Adv or a ScanRsp has been received.
This event comes with a message of GapScan_Evt_AdvRpt_t. Application is responsible for freeing both the message and the message data (msg->pData).
| #define GAP_EVT_ADV_REPORT_FULL (uint32_t)BV(23) |
Maximum number of Adv reports have been recorded.
This event comes with a message of GapScan_Evt_AdvRpt_t.
| #define GAP_EVT_ADV_SET_TERMINATED (uint32_t)BV(4) |
Sent when an advertisement set is terminated due to a connection establishment
pBuf should be cast to GapAdv_setTerm_t
| #define GAP_EVT_ADV_START (uint32_t)BV(2) |
Sent at the beginning of each advertisement (for legacy advertising) or at the beginning of each each advertisement set (for extended advertising)
pBuf should be cast to a uint8_t which will contain the advertising handle
| #define GAP_EVT_ADV_START_AFTER_ENABLE (uint32_t)BV(0) |
Sent on the first advertisement after a GapAdv_enable
pBuf should be cast to a uint8_t which will contain the advertising handle
| #define GAP_EVT_SCAN_DISABLED (uint32_t)BV(17) |
Scanner has been disabled.
This event comes with a message of GapScan_Evt_End_t. Application is responsible for freeing the message.
| #define GAP_EVT_SCAN_EVT_MASK |
Mask for all scan events.
| #define GAP_EVT_SCAN_INT_ENDED (uint32_t)BV(20) |
Scan interval has ended.
Possibly a new scan interval and a new scan window have started.
| #define GAP_EVT_SCAN_PRD_ENDED (uint32_t)BV(18) |
Scan period has ended.
Possibly a new scan period and a new scan duration have started.
| #define GAP_EVT_SCAN_REQ_RECEIVED (uint32_t)BV(5) |
Sent when a scan request is received
pBuf should be cast to GapAdv_scanReqReceived_t