CC23x0R5DriverLibrary
|
#include "uart.h"
Functions | |
void | UARTConfigSetExpClk (uint32_t base, uint32_t UARTClkFreq, uint32_t baudFreq, uint32_t config) |
Sets the configuration of a UART. More... | |
void | UARTDisable (uint32_t base) |
Disables transmitting and receiving. More... | |
uint8_t | UARTGetChar (uint32_t base) |
Waits for a character from the specified port. More... | |
void | UARTPutChar (uint32_t base, uint8_t data) |
Waits to send a character to the specified port. More... | |