ANSIX936KDF Parameters. More...
#include <ANSIX936KDF.h>
Data Fields | |
ANSIX936KDF_ReturnBehavior | returnBehavior |
uint32_t | timeout |
ANSIX936KDF Parameters.
ANSIX936KDF Parameters are used to with the ANSIX936KDF_open() call. Default values for these parameters are set using ANSIX936KDF_Params_init().
ANSIX936KDF_ReturnBehavior ANSIX936KDF_Params::returnBehavior |
Blocking or polling return behavior
uint32_t ANSIX936KDF_Params::timeout |
Timeout before the driver returns an error in ANSIX936KDF_RETURN_BEHAVIOR_BLOCKING