ECIES Parameters. More...
#include <ECIES.h>
Data Fields | |
ECIES_ReturnBehavior | returnBehavior |
uint32_t | timeout |
ECIES Parameters.
ECIES Parameters are used to with the ECIES_open() call. Default values for these parameters are set using ECIES_Params_init().
ECIES_ReturnBehavior ECIES_Params::returnBehavior |
Blocking or polling return behavior
uint32_t ECIES_Params::timeout |
Timeout before the driver returns an error in ECIES_RETURN_BEHAVIOR_BLOCKING