Contains part of the GAP Bond Manager Parameters values.
More...
|
uint8_t | authenPairingOnly |
|
uint8_t | autoSyncAL |
|
uint8_t | bondFailAction |
|
uint8_t | bonding |
|
uint8_t | eccDebugKeys |
|
uint8_t | eccReGenPolicy |
|
uint8_t | eraseBondWhileInConn |
|
uint8_t | ioCap |
|
uint8_t | KeyDistList |
|
uint8_t | KeySize |
|
uint8_t | mitm |
|
uint8_t | pairMode |
|
uint8_t | removeLRUBond |
|
uint8_t | sameIrkAction |
|
uint8_t | secureConnection |
|
Contains part of the GAP Bond Manager Parameters values.
The documentation for this struct was generated from the following file: