|
| #define | ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_REQ(data_buf, group_member_req) |
| | Parses Get Group Membership command and returns pointer to data request structure. If request contains invalid data, NULL is returned. More...
|
| |
| #define | ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_RES(data_buf, group_member_res) |
| | Parses Get Group Membership command response and returns pointer to data response structure. If response contains invalid data, NULL is returned. More...
|
| |
| #define | ZB_ZCL_GROUPS_INIT_GET_GROUP_MEMBERSHIP_REQ(buffer, ptr, def_resp, group_cnt) |
| | Initialize Get group membership command. More...
|
| |
| #define | ZB_ZCL_GROUPS_ADD_ID_GET_GROUP_MEMBERSHIP_REQ(ptr, group_id) |
| | Add group id to command payload. More...
|
| |
| #define | ZB_ZCL_GROUPS_SEND_GET_GROUP_MEMBERSHIP_REQ( buffer, ptr, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb) |
| | Sends Get group membership command. More...
|
| |
Both Get Group Membership command request and response have a complex array-style payload.
- Examples
- Get Group Membership request can be filled in as:
§ ZB_ZCL_GROUPS_ADD_ID_GET_GROUP_MEMBERSHIP_REQ
| #define ZB_ZCL_GROUPS_ADD_ID_GET_GROUP_MEMBERSHIP_REQ |
( |
|
ptr, |
|
|
|
group_id |
|
) |
| |
§ ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_REQ
| #define ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_REQ |
( |
|
data_buf, |
|
|
|
group_member_req |
|
) |
| |
#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_groups.h>
Value:{ \
zb_uint8_t i_tmp; \
zb_uint8_t cmd_size = ZB_ZCL_GET_GROUP_MEMBERSHIP_REQ_SIZE; \
\
(group_member_req) = (
zb_buf_len(data_buf) >= cmd_size) ? \
\
if (group_member_req) \
{ \
cmd_size +=
sizeof(
zb_uint16_t) * (group_member_req)->group_count; \
{ \
for(i_tmp = 0; i_tmp < (group_member_req)->group_count; i_tmp++) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(group_member_req)->group_id[i_tmp]); \
} \
} \
else \
{ \
group_member_req = NULL; \
} \
} \
}
Get Group Membership command structure.
Definition: zb_zcl_groups.h:382
unsigned short zb_uint16_t
Project-local 2-byte unsigned int type.
Definition: zb_types.h:151
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372
Parses Get Group Membership command and returns pointer to data request structure. If request contains invalid data, NULL is returned.
- Parameters
-
| data_buf | - pointer to zb_buf_t buffer containing command request data |
| group_member_req | - pointer to command request |
- Note
- data_buf buffer should contain command request payload without ZCL header.
§ ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_RES
| #define ZB_ZCL_GROUPS_GET_GROUP_MEMBERSHIP_RES |
( |
|
data_buf, |
|
|
|
group_member_res |
|
) |
| |
#include </home/developer/.conan/data/ti_zigbee/1.00.00.40/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_groups.h>
Value:{ \
zb_uint8_t i; \
zb_uint8_t cmd_size = ZB_ZCL_GET_GROUP_MEMBERSHIP_RES_SIZE; \
\
(group_member_res) = (
zb_buf_len(data_buf) >= cmd_size) ? \
\
if (group_member_res) \
{ \
cmd_size +=
sizeof(
zb_uint16_t) * (group_member_res)->group_count; \
{ \
for(i = 0; i < (group_member_res)->group_count; i++) \
{ \
ZB_ZCL_HTOLE16_INPLACE(&(group_member_res)->group_id[i]); \
} \
} \
else \
{ \
group_member_res = NULL; \
} \
} \
}
unsigned short zb_uint16_t
Project-local 2-byte unsigned int type.
Definition: zb_types.h:151
Get Group Membership command response structure.
Definition: zb_zcl_groups.h:429
#define zb_buf_begin(buf)
Definition: zboss_api_buf.h:354
#define zb_buf_len(buf)
Definition: zboss_api_buf.h:372
Parses Get Group Membership command response and returns pointer to data response structure. If response contains invalid data, NULL is returned.
- Parameters
-
| data_buf | - pointer to zb_buf_t buffer containing command response data |
| group_member_res | - pointer to command response |
- Note
- data_buf buffer should contain command response payload without ZCL header.
§ ZB_ZCL_GROUPS_INIT_GET_GROUP_MEMBERSHIP_REQ
| #define ZB_ZCL_GROUPS_INIT_GET_GROUP_MEMBERSHIP_REQ |
( |
|
buffer, |
|
|
|
ptr, |
|
|
|
def_resp, |
|
|
|
group_cnt |
|
) |
| |
§ ZB_ZCL_GROUPS_SEND_GET_GROUP_MEMBERSHIP_REQ
| #define ZB_ZCL_GROUPS_SEND_GET_GROUP_MEMBERSHIP_REQ |
( |
|
buffer, |
|
|
|
ptr, |
|
|
|
addr, |
|
|
|
dst_addr_mode, |
|
|
|
dst_ep, |
|
|
|
ep, |
|
|
|
prfl_id, |
|
|
|
cb |
|
) |
| |
§ zb_zcl_groups_get_group_membership_req_t
§ zb_zcl_groups_get_group_membership_res_t