|
#define | SPI_DMA_DONE_TX SPI_IMASK_DMATX |
| DMA Done 1 event for TX event mask. More...
|
|
#define | SPI_DMA_DONE_RX SPI_IMASK_DMARX |
| DMA Done 1 event for RX event mask. More...
|
|
#define | SPI_IDLE SPI_IMASK_IDLE |
| SPI Idle event mask. More...
|
|
#define | SPI_TXEMPTY SPI_IMASK_TXEMPTY |
| Transmit FIFO Empty event mask. More...
|
|
#define | SPI_TX SPI_IMASK_TX |
| Transmit FIFO event mask. More...
|
|
#define | SPI_RX SPI_IMASK_RX |
| Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached. More...
|
|
#define | SPI_RTOUT SPI_IMASK_RTOUT |
| Enable SPI Receive Time-Out event mask. More...
|
|
#define | SPI_PER SPI_IMASK_PER |
| Parity error event mask. More...
|
|
#define | SPI_RXFIFO_OVF SPI_IMASK_RXOVF |
| RXFIFO overflow event mask. More...
|
|
#define | SPI_BUSY SPI_STA_BUSY_ACTIVE |
| Busy. More...
|
|
#define | SPI_RX_NOT_FULL SPI_STA_RNF_NOT_FULL |
| Receive FIFO not full. More...
|
|
#define | SPI_RX_EMPTY SPI_STA_RFE_EMPTY |
| Receive FIFO empty. More...
|
|
#define | SPI_TX_NOT_FULL SPI_STA_TNF_NOT_FULL |
| Transmit FIFO not full. More...
|
|
#define | SPI_TX_EMPTY SPI_STA_TFE_EMPTY |
| Transmit FIFO empty. More...
|
|
#define | SPI_STATUS_MASK 0x0000001F |
| Mask for bits above. More...
|
|
#define | SPI_FRF_MOTO_MODE_0 (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST) |
| Motorola format 3-wire, polarity 0, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_1 (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND) |
| Motorola format 3-wire, polarity 0, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_2 (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST) |
| Motorola format 3-wire, polarity 1, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_3 (SPI_CTL0_FRF_MOTOROLA_3WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND) |
| Motorola format 3-wire, polarity 1, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_4 (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_FIRST) |
| Motorola format 4-wire, polarity 0, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_5 (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_LO | SPI_CTL0_SPH_SECOND) |
| Motorola format 4-wire, polarity 0, phase 1. More...
|
|
#define | SPI_FRF_MOTO_MODE_6 (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_FIRST) |
| Motorola format 4-wire, polarity 1, phase 0. More...
|
|
#define | SPI_FRF_MOTO_MODE_7 (SPI_CTL0_FRF_MOTOROLA_4WIRE | SPI_CTL0_SPO_HI | SPI_CTL0_SPH_SECOND) |
| Motorola format 4-wire, polarity 1, phase 1. More...
|
|
#define | SPI_FRF_TI SPI_CTL0_FRF_TI_SYNC |
| TI Sync frame format. More...
|
|
#define | SPI_FRF_NMW SPI_CTL0_FRF_MIRCOWIRE |
| MicroWire frame format. More...
|
|
#define | SPI_MODE_CONTROLLER SPI_CTL1_MS_CONTROLLER |
| SPI controller. More...
|
|
#define | SPI_MODE_PERIPHERAL SPI_CTL1_MS_PERIPHERAL |
| SPI peripheral. More...
|
|
#define | SPI_MODE_PERIPHERAL_OD SPI_CTL1_SOD_ENABLE |
| output disabled More...
|
|
#define | SPI_DMA_TX SPI_DMACR_TXEN |
| Enable DMA for transmit. More...
|
|
#define | SPI_DMA_RX SPI_DMACR_RXEN |
| Enable DMA for receive. More...
|
|
|
void | SPIConfigSetExpClk (uint32_t base, uint32_t spiClk, uint32_t protocol, uint32_t mode, uint32_t bitRate, uint32_t dataWidth) |
| Configures the serial peripheral port. More...
|
|
__STATIC_INLINE void | SPIEnable (uint32_t base) |
| Enables the serial peripheral port. More...
|
|
__STATIC_INLINE void | SPIDisable (uint32_t base) |
| Disables the serial peripheral port. More...
|
|
void | SPIPutData (uint32_t base, uint32_t data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
int32_t | SPIPutDataNonBlocking (uint32_t base, uint32_t data) |
| Puts a data element into the SPI transmit FIFO. More...
|
|
void | SPIGetData (uint32_t base, uint32_t *data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
int32_t | SPIGetDataNonBlocking (uint32_t base, uint32_t *data) |
| Gets a data element from the SPI receive FIFO. More...
|
|
__STATIC_INLINE bool | SPIBusy (uint32_t base) |
| Determines whether the SPI transmitter is busy or not. More...
|
|
__STATIC_INLINE uint32_t | SPIStatus (uint32_t base) |
| Get the status of the SPI data buffers. More...
|
|
void | SPIRegisterInt (uint32_t base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|
void | SPIUnregisterInt (uint32_t base) |
| Unregisters an interrupt handler for the Serial Peripheral Interface in the dynamic interrupt table. More...
|
|
__STATIC_INLINE void | SPIEnableInt (uint32_t base, uint32_t intFlags) |
| Enables individual SPI interrupt sources. More...
|
|
__STATIC_INLINE void | SPIDisableInt (uint32_t base, uint32_t intFlags) |
| Disables individual SPI interrupt sources. More...
|
|
__STATIC_INLINE void | SPIClearInt (uint32_t base, uint32_t intFlags) |
| Clears SPI interrupt sources. More...
|
|
__STATIC_INLINE uint32_t | SPIIntStatus (uint32_t base, bool isMasked) |
| Gets the current interrupt status. More...
|
|
__STATIC_INLINE void | SPIEnableDMA (uint32_t base, uint32_t dmaFlags) |
| Enable SPI DMA operation. More...
|
|
__STATIC_INLINE void | SPIDisableDMA (uint32_t base, uint32_t dmaFlags) |
| Disable SPI DMA operation. More...
|
|