CC27xxDriverLibrary
systick.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_ints.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_systick.h"
#include "debug.h"
#include "interrupt.h"
Include dependency graph for systick.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Functions

__STATIC_INLINE void SysTickEnable (void)
 Enables the SysTick counter. More...
 
__STATIC_INLINE void SysTickDisable (void)
 Disables the SysTick counter. More...
 
__STATIC_INLINE void SysTickRegisterInt (void(*pfnHandler)(void))
 Registers an interrupt handler for the SysTick interrupt in the dynamic interrupt table. More...
 
__STATIC_INLINE void SysTickUnregisterInt (void)
 Unregisters the interrupt handler for the SysTick interrupt in the dynamic interrupt table. More...
 
__STATIC_INLINE void SysTickEnableInt (void)
 Enables the SysTick interrupt. More...
 
__STATIC_INLINE void SysTickDisableInt (void)
 Disables the SysTick interrupt. More...
 
__STATIC_INLINE void SysTickSetPeriod (uint32_t period)
 Sets the period of the SysTick counter. More...
 
__STATIC_INLINE uint32_t SysTickGetPeriod (void)
 Gets the period of the SysTick counter. More...
 
__STATIC_INLINE uint32_t SysTickGetValue (void)
 Gets the current value of the SysTick counter. More...