![]() |
![]() |
TI BLE5-Stack API Documentation
9.11.01
|
Data Fields | |
uint8_t | ch3CJump |
one of the valid CSChannelJump values More... | |
uint8_t | ch3cShape |
selected shape to be rendered More... | |
csChm_t | channelMap |
channel map csChm_t More... | |
uint8_t | chMRepetition |
number of times the ChM field will be cycled through More... | |
uint8_t | chSel |
channel selection algorithm to be used CS_Chan_Sel_Alg More... | |
uint8_t | configId |
CS configuration ID. More... | |
uint16_t | connHandle |
connection handle More... | |
csEventOpcodes_e | csEvtOpcode |
CS Event Code. More... | |
uint8_t | csStatus |
Event status. More... | |
uint8_t | csSyncPhy |
transmit and receive PHY to be used CS_Sync_Phy_Supported More... | |
uint8_t | mainMode |
which CS modes are to be used CS_Mode More... | |
uint8_t | mainModeMaxSteps |
a Sub_Mode step is executed More... | |
uint8_t | mainModeMinSteps |
range of Main_Mode steps to be executed before More... | |
uint8_t | mainModeRepetition |
num of main mode steps from the last CS subevent to be repeated More... | |
uint8_t | modeZeroSteps |
number of mode 0 steps to be included at the beginning of each CS Subevent More... | |
uint8_t | rfu0 |
reserved for future use More... | |
uint8_t | rfu1 |
reserved for future use More... | |
uint8_t | role |
initiator or reflector CS_Role More... | |
uint8_t | rttType |
which RTT variant is to be used CS_RTT_Type More... | |
uint8_t | state |
0b00 disabled, 0b01 enabled More... | |
uint8_t | subMode |
which CS modes are to be used CS_Mode More... | |
uint8_t | tFCs |
Index used for frequency changes. More... | |
uint8_t | tIP1 |
Index of the period used between RTT packets. More... | |
uint8_t | tIP2 |
Index of the interlude period used between CS tones. More... | |
uint8_t | tPM |
Index for the measurement period of CS tones. More... | |
uint8_t ch3CJump |
one of the valid CSChannelJump values
uint8_t ch3cShape |
selected shape to be rendered
csChm_t channelMap |
channel map csChm_t
uint8_t chMRepetition |
number of times the ChM field will be cycled through
uint8_t chSel |
channel selection algorithm to be used CS_Chan_Sel_Alg
uint8_t configId |
CS configuration ID.
uint16_t connHandle |
connection handle
csEventOpcodes_e csEvtOpcode |
CS Event Code.
uint8_t csStatus |
Event status.
uint8_t csSyncPhy |
transmit and receive PHY to be used CS_Sync_Phy_Supported
uint8_t mainMode |
which CS modes are to be used CS_Mode
uint8_t mainModeMaxSteps |
a Sub_Mode step is executed
uint8_t mainModeMinSteps |
range of Main_Mode steps to be executed before
uint8_t mainModeRepetition |
num of main mode steps from the last CS subevent to be repeated
uint8_t modeZeroSteps |
number of mode 0 steps to be included at the beginning of each CS Subevent
uint8_t rfu0 |
reserved for future use
uint8_t rfu1 |
reserved for future use
uint8_t role |
initiator or reflector CS_Role
uint8_t rttType |
which RTT variant is to be used CS_RTT_Type
uint8_t state |
0b00 disabled, 0b01 enabled
uint8_t subMode |
which CS modes are to be used CS_Mode
uint8_t tFCs |
Index used for frequency changes.
uint8_t tIP1 |
Index of the period used between RTT packets.
uint8_t tIP2 |
Index of the interlude period used between CS tones.
uint8_t tPM |
Index for the measurement period of CS tones.