![]() |
![]() |
TI BLE5-Stack API Documentation
9.11.01
|
GATT Structure for Characteristic Presentation Format Value. More...
Data Fields | |
uint16 | desc |
Description of this attribute as defined in a higher layer profile. More... | |
int8 | exponent |
A sign integer which represents the exponent of an integer. More... | |
uint8 | format |
Format of the value of this characteristic. More... | |
uint8 | nameSpace |
Name space of the description. More... | |
uint16 | unit |
Unit of this attribute as defined in the data dictionary. More... | |
GATT Structure for Characteristic Presentation Format Value.
uint16 desc |
Description of this attribute as defined in a higher layer profile.
int8 exponent |
A sign integer which represents the exponent of an integer.
uint8 format |
Format of the value of this characteristic.
uint8 nameSpace |
Name space of the description.
uint16 unit |
Unit of this attribute as defined in the data dictionary.