TI BLE5-Stack API Documentation  9.11.01
Data Fields
hciEvt_BLERemoteConnParamReq_t Struct Reference

LE Remote Connection Parameter Request Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code. More...
 
uint16 connHandle
 connection handle More...
 
osal_event_hdr_t hdr
 osal event header More...
 
uint16 Interval_Max
 maximum connection interval More...
 
uint16 Interval_Min
 minimum connection interval More...
 
uint16 Latency
 peripheral latency More...
 
uint8 status
 status of event More...
 
uint16 Timeout
 supervision timeout More...
 

Detailed Description

LE Remote Connection Parameter Request Event.

Field Documentation

§ BLEEventCode

uint8 BLEEventCode

BLE Event Code.

§ connHandle

uint16 connHandle

connection handle

§ hdr

osal event header

§ Interval_Max

uint16 Interval_Max

maximum connection interval

§ Interval_Min

uint16 Interval_Min

minimum connection interval

§ Latency

uint16 Latency

peripheral latency

§ status

uint8 status

status of event

§ Timeout

uint16 Timeout

supervision timeout


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale