![]() |
![]() |
TI BLE5-Stack API Documentation
9.11.01
|
PSM information format. More...
Data Fields | |
uint16 | initPeerCredits |
Number of LE-frames that peer device can send. More... | |
uint8 | maxNumChannels |
Maximum number of CO Channels supported by PSM. More... | |
uint16 | mps |
Maximum payload size that can be received by local device. More... | |
uint16 | mtu |
Maximum SDU size that can be received by local device. More... | |
uint8 | numActiveChannels |
Number of active CO Channels. More... | |
uint16 | peerCreditThreshold |
Low threshold for number of peer credits. More... | |
PSM information format.
uint16 initPeerCredits |
Number of LE-frames that peer device can send.
uint8 maxNumChannels |
Maximum number of CO Channels supported by PSM.
uint16 mps |
Maximum payload size that can be received by local device.
uint16 mtu |
Maximum SDU size that can be received by local device.
uint8 numActiveChannels |
Number of active CO Channels.
uint16 peerCreditThreshold |
Low threshold for number of peer credits.