CANMCAN.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2023-2024, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file CANMCAN.h
34  *
35  * @brief Common CAN functions for MCAN configuration
36  *******************************************************************************
37  */
38 
39 #ifndef ti_drivers_can_common_canmcan__include
40 #define ti_drivers_can_common_canmcan__include
41 
42 #include <stdint.h>
43 #include <ti/drivers/CAN.h>
44 #include <third_party/mcan/MCAN.h>
45 
46 #ifdef __cplusplus
47 extern "C" {
48 #endif
49 
53 #define MCAN_INT_SRC_RX_MASK \
54  ((uint32_t)MCAN_INT_SRC_RX_FIFO0_NEW_MSG | (uint32_t)MCAN_INT_SRC_RX_FIFO1_NEW_MSG | \
55  (uint32_t)MCAN_INT_SRC_DEDICATED_RX_BUFF_MSG)
56 
65 int_fast16_t CANMCAN_setBitTimingRaw(const CAN_BitRateTimingRaw *rawTiming);
66 
81 int_fast16_t CANMCAN_configMsgRam(const CAN_MsgRamConfig *config, uint32_t msgRamSize, bool enableCANFD);
82 
90 uint32_t CANMCAN_getInterruptMask(uint32_t eventMask);
91 
92 #ifdef __cplusplus
93 }
94 #endif
95 
96 #endif /* ti_drivers_can_common_canmcan__include */
Controller Area Network (CAN) Driver Interface.
uint32_t CANMCAN_getInterruptMask(uint32_t eventMask)
Returns the MCAN interrupt mask based on the CAN event mask.
CAN Message RAM configuration.
Definition: CAN.h:619
int_fast16_t CANMCAN_configMsgRam(const CAN_MsgRamConfig *config, uint32_t msgRamSize, bool enableCANFD)
Configures the MCAN message RAM.
int_fast16_t CANMCAN_setBitTimingRaw(const CAN_BitRateTimingRaw *rawTiming)
Sets the MCAN raw bit timing.
Structure defining the raw MCAN bit rate configuration.
Definition: CAN.h:699
Hardware abstraction layer for M_CAN Controller v3.2.1.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale