Data Fields
CAN_MsgRamConfig Struct Reference

CAN Message RAM configuration. More...

#include <CAN.h>

Collaboration diagram for CAN_MsgRamConfig:
Collaboration graph
[legend]

Data Fields

uint32_t stdFilterNum
 
uint32_t extFilterNum
 
MCAN_StdMsgIDFilterElementstdMsgIDFilterList
 
MCAN_ExtMsgIDFilterElementextMsgIDFilterList
 
uint32_t rxFifoNum [2]
 
uint32_t rxBufNum
 
uint32_t txBufNum
 
uint32_t txFifoQNum
 
uint32_t txFifoQMode
 
uint32_t txEventFifoNum
 

Detailed Description

CAN Message RAM configuration.

The CAN_MsgRamConfig structure contains information used to configure the message RAM.

This structure needs to be defined before calling CAN_init() and it must not be changed thereafter.

See also
CAN_init()

Field Documentation

§ stdFilterNum

uint32_t CAN_MsgRamConfig::stdFilterNum

Number of Standard ID filter elements [0-128]

§ extFilterNum

uint32_t CAN_MsgRamConfig::extFilterNum

Number of Extended ID filter elements [0-64]

§ stdMsgIDFilterList

MCAN_StdMsgIDFilterElement* CAN_MsgRamConfig::stdMsgIDFilterList

Points to Standard ID filter elements. Set to NULL if zero elements.

§ extMsgIDFilterList

MCAN_ExtMsgIDFilterElement* CAN_MsgRamConfig::extMsgIDFilterList

Points to Extended ID filter elements. Set to NULL if zero elements.

§ rxFifoNum

uint32_t CAN_MsgRamConfig::rxFifoNum[2]

Number of Rx FIFO elements [0-64] for FIFO0 and FIFO1 respectively

§ rxBufNum

uint32_t CAN_MsgRamConfig::rxBufNum

Number of dedicated Rx Buffer elements [0-64]

§ txBufNum

uint32_t CAN_MsgRamConfig::txBufNum

Number of dedicated Tx Buffer elements [0-64]

§ txFifoQNum

uint32_t CAN_MsgRamConfig::txFifoQNum

Number of Tx buffer elements [0-64] for Tx FIFO or Queue

§ txFifoQMode

uint32_t CAN_MsgRamConfig::txFifoQMode

Tx FIFO/Queue Mode: 0 = Tx FIFO mode, 1 = Tx Queue mode

§ txEventFifoNum

uint32_t CAN_MsgRamConfig::txEventFifoNum

Number of Tx Event FIFO elements [0-32]


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale