![]() |
![]() |
Clock interface for the RTOS Porting Interface.
============================================================================
The ClockP module can be used to schedule functions that run at intervals specified in the underlying kernel's system ticks. ClockP instances are one-shot. The one-shot function will be run once after the specified period has elapsed since calling ClockP_start().
The ClockP module can also be used to obtain the period of the kernel's system tick in micro seconds. This is useful for determining the number of ticks needed for setting a Clock object's period.
When using the TI-RTOS kernel, ClockP functions are run at software interrupt level. With FreeRTOS, the ClockP functions are either run by a timer service task with priority configured by the application, or in hardware interrupt directly, depending on the device platform.
#include <stdint.h>#include <stdbool.h>#include <stddef.h>

Go to the source code of this file.
Data Structures | |
| union | ClockP_Struct |
| ClockP structure. More... | |
| struct | ClockP_FreqHz |
| Frequency-in-hertz struct. More... | |
| struct | ClockP_Params |
| Basic ClockP Parameters. More... | |
Macros | |
| #define | ClockP_STRUCT_SIZE (68) |
| Number of bytes greater than or equal to the size of any RTOS ClockP object. More... | |
| #define | ClockP_handle(x) ((ClockP_Handle)(x)) |
Typedefs | |
| typedef union ClockP_Struct | ClockP_Struct |
| ClockP structure. More... | |
| typedef void * | ClockP_Handle |
| Opaque client reference to an instance of a ClockP. More... | |
| typedef void(* | ClockP_Fxn) (uintptr_t arg) |
| Prototype for a ClockP callback function. More... | |
Enumerations | |
| enum | ClockP_Status { ClockP_OK = 0, ClockP_FAILURE = -1 } |
| Status codes for ClockP APIs. More... | |
Functions | |
| ClockP_Handle | ClockP_construct (ClockP_Struct *clockP, ClockP_Fxn clockFxn, uint32_t timeout, ClockP_Params *params) |
| Function to construct a clock object. More... | |
| void | ClockP_destruct (ClockP_Struct *clockP) |
| Function to destruct a clock object. More... | |
| ClockP_Handle | ClockP_create (ClockP_Fxn clockFxn, uint32_t timeout, ClockP_Params *params) |
| Function to create a clock object. More... | |
| void | ClockP_delete (ClockP_Handle handle) |
| Function to delete a clock. More... | |
| void | ClockP_getCpuFreq (ClockP_FreqHz *freq) |
| Get CPU frequency in Hertz. More... | |
| uint32_t | ClockP_getSystemTickPeriod (void) |
| Get the system tick period in number of micro seconds. More... | |
| uint32_t | ClockP_getSystemTicks (void) |
| Get the current tick value in number of system ticks. More... | |
| uint64_t | ClockP_getSystemTicks64 (void) |
| Get the current tick value in number of system ticks. More... | |
| uint32_t | ClockP_getTicksUntilInterrupt (void) |
| Get number of ClockP tick periods expected to expire between now and the next interrupt from the timer peripheral. More... | |
| uint32_t | ClockP_getTimeout (ClockP_Handle handle) |
| Get timeout of clock instance. More... | |
| bool | ClockP_isActive (ClockP_Handle handle) |
| Determine if a clock object is currently active (i.e., running) More... | |
| void | ClockP_Params_init (ClockP_Params *params) |
| Initialize params structure to default values. More... | |
| void | ClockP_setFunc (ClockP_Handle handle, ClockP_Fxn clockFxn, uintptr_t arg) |
| Function to overwrite ClockP callback function and arg. More... | |
| void | ClockP_setTimeout (ClockP_Handle handle, uint32_t timeout) |
| Set the initial timeout. More... | |
| void | ClockP_setPeriod (ClockP_Handle handle, uint32_t period) |
| Set the clock period. More... | |
| void | ClockP_start (ClockP_Handle handle) |
| Function to start a clock. More... | |
| void | ClockP_stop (ClockP_Handle handle) |
| Function to stop a clock. More... | |
| void | ClockP_usleep (uint32_t usec) |
| Set delay in micro seconds. More... | |
| void | ClockP_sleep (uint32_t sec) |
| Set delay in seconds. More... | |
| #define ClockP_STRUCT_SIZE (68) |
Number of bytes greater than or equal to the size of any RTOS ClockP object.
NoRTOS: 32 (biggest of the HW-specific ClockP instance structs) BIOS 6.x: 40 BIOS 7.x: 36 FreeRTOS: 68
| #define ClockP_handle | ( | x | ) | ((ClockP_Handle)(x)) |
| typedef union ClockP_Struct ClockP_Struct |
ClockP structure.
Opaque structure that should be large enough to hold any of the RTOS specific ClockP objects.
| typedef void* ClockP_Handle |
Opaque client reference to an instance of a ClockP.
A ClockP_Handle returned from ClockP_create() or ClockP_construct() represents that instance. It is then is used in the other instance based functions (e.g. ClockP_start(), ClockP_stop(), etc.).
| typedef void(* ClockP_Fxn) (uintptr_t arg) |
Prototype for a ClockP callback function.
| enum ClockP_Status |
| ClockP_Handle ClockP_construct | ( | ClockP_Struct * | clockP, |
| ClockP_Fxn | clockFxn, | ||
| uint32_t | timeout, | ||
| ClockP_Params * | params | ||
| ) |
Function to construct a clock object.
| clockP | Pointer to ClockP_Struct object. |
| timeout | The startup timeout, if supported by the RTOS. |
| clockFxn | Function called when timeout or period expires. |
| params | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The ClockP default parameters are noted in ClockP_Params_init(). |
| void ClockP_destruct | ( | ClockP_Struct * | clockP | ) |
Function to destruct a clock object.
| clockP | Pointer to a ClockP_Struct object that was passed to ClockP_construct(). |
The clock object must be stopped before calling destruct.
| ClockP_Handle ClockP_create | ( | ClockP_Fxn | clockFxn, |
| uint32_t | timeout, | ||
| ClockP_Params * | params | ||
| ) |
Function to create a clock object.
This function will allocate memory for the instance's ClockP_Struct.
| clockFxn | Function called when timeout or period expires. |
| timeout | The startup timeout, if supported by the RTOS. |
| params | Pointer to the instance configuration parameters. NULL denotes to use the default parameters. The ClockP default parameters are noted in ClockP_Params_init(). |
| void ClockP_delete | ( | ClockP_Handle | handle | ) |
Function to delete a clock.
| handle | A ClockP_Handle returned from ClockP_create() |
The clock object must be stopped before calling delete.
| void ClockP_getCpuFreq | ( | ClockP_FreqHz * | freq | ) |
Get CPU frequency in Hertz.
| freq | Pointer to the FreqHz structure |
| uint32_t ClockP_getSystemTickPeriod | ( | void | ) |
Get the system tick period in number of micro seconds.
| uint32_t ClockP_getSystemTicks | ( | void | ) |
Get the current tick value in number of system ticks.
The value returned will wrap back to zero after it reaches the max value that can be stored in 32 bits.
| uint64_t ClockP_getSystemTicks64 | ( | void | ) |
Get the current tick value in number of system ticks.
The value returned will wrap back to zero after it reaches the max value that can be stored in 64 bits.
| uint32_t ClockP_getTicksUntilInterrupt | ( | void | ) |
Get number of ClockP tick periods expected to expire between now and the next interrupt from the timer peripheral.
Returns the number of ClockP tick periods that are expected to expire between now and the next interrupt from the timer peripheral.
Used internally by various Power modules
| uint32_t ClockP_getTimeout | ( | ClockP_Handle | handle | ) |
Get timeout of clock instance.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
Returns the remaining time in clock ticks if the instance has been started. If the clock is not active, the initial timeout value is returned.
| bool ClockP_isActive | ( | ClockP_Handle | handle | ) |
Determine if a clock object is currently active (i.e., running)
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
Returns true if the clock object is currently active, otherwise returns false.
| void ClockP_Params_init | ( | ClockP_Params * | params | ) |
Initialize params structure to default values.
The default parameters are:
| params | Pointer to the configuration parameters instance. |
| void ClockP_setFunc | ( | ClockP_Handle | handle, |
| ClockP_Fxn | clockFxn, | ||
| uintptr_t | arg | ||
| ) |
Function to overwrite ClockP callback function and arg.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
| clockFxn | Function called when timeout or period expires. |
| arg | Argument passed to clockFxn |
| void ClockP_setTimeout | ( | ClockP_Handle | handle, |
| uint32_t | timeout | ||
| ) |
Set the initial timeout.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
| timeout | Initial timeout in ClockP ticks |
Cannot be used to set the initial timeout if the clock has been started.
| void ClockP_setPeriod | ( | ClockP_Handle | handle, |
| uint32_t | period | ||
| ) |
Set the clock period.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
| period | Periodic interval in ClockP ticks |
Cannot be used to set the clock period to zero.
| void ClockP_start | ( | ClockP_Handle | handle | ) |
Function to start a clock.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
| void ClockP_stop | ( | ClockP_Handle | handle | ) |
Function to stop a clock.
| handle | A ClockP_Handle returned from ClockP_create() or ClockP_construct() |
It is ok to call ClockP_stop() for a clock that has not been started.
| void ClockP_usleep | ( | uint32_t | usec | ) |
Set delay in micro seconds.
| usec | A duration in micro seconds |
| void ClockP_sleep | ( | uint32_t | sec | ) |
Set delay in seconds.
| sec | A duration in seconds |