Data Fields
ADCBufLPF3_AdcChannelLutEntry Struct Reference

Table entry that maps a virtual adc channel to the corresponding hardware configuration. More...

#include <ADCBufLPF3.h>

Data Fields

uint_fast32_t refVoltage
 
uint8_t adcInputDIO
 
uint8_t internalChannel
 
ADCLPF3_Reference_Source refSource
 

Detailed Description

Table entry that maps a virtual adc channel to the corresponding hardware configuration.

Field Documentation

§ refVoltage

uint_fast32_t ADCBufLPF3_AdcChannelLutEntry::refVoltage

Reference voltage of the selected reference source in microvolts

§ adcInputDIO

uint8_t ADCBufLPF3_AdcChannelLutEntry::adcInputDIO

DIO that this virtual channel is routed to. Should be set to GPIO_INVALID_INDEX if internal signal is used.

§ internalChannel

uint8_t ADCBufLPF3_AdcChannelLutEntry::internalChannel

Internal signal routed to ADC

§ refSource

ADCLPF3_Reference_Source ADCBufLPF3_AdcChannelLutEntry::refSource

Reference source for the ADC to use


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale