![]() |
![]() |
LogSinkTraceLPF3 global configuration. More...
#include <LogSinkTraceLPF3.h>
Data Fields | |
| uint32_t | tracerConfig |
| uint32_t | lrfdTracerPin |
| int32_t | tracerPinMux |
| uint32_t | tracerPin |
LogSinkTraceLPF3 global configuration.
The LogSinkTraceLPF3_Config structure contains settings used to configure RFtracer.
The tracerConfig member needs a 3 element combination of the configuration defines above put together with an OR operation. A valid configuration would be: tracerConfig = LogSinkTraceLPF3_CHANNELS_RADIO_ONLY | LogSinkTraceLPF3_TIMESTAMP_ENABLED | LogSinkTraceLPF3_PRESCALER_DIV3 LRFDTRC_CFG_PRESCAL_DIV3
lrfdTracerPin, tracerPinMux, tracerPin are all settings needed for the internal muxing of the tracer pin.
| uint32_t LogSinkTraceLPF3_Config::tracerConfig |
Configuration for tracer
| uint32_t LogSinkTraceLPF3_Config::lrfdTracerPin |
LRFD tracer pin for the LRF muxing
| int32_t LogSinkTraceLPF3_Config::tracerPinMux |
Tracer PIN mux value
| uint32_t LogSinkTraceLPF3_Config::tracerPin |
DIO pin for the tracer