Data Fields
SDFatFS_Config Struct Reference

SDFatFS Global configuration. More...

#include <SDFatFS.h>

Collaboration diagram for SDFatFS_Config:
Collaboration graph
[legend]

Data Fields

SDFatFS_Objectobject
 

Detailed Description

SDFatFS Global configuration.

The SDFatFS_Config structure contains a single pointer used to characterize the SDFatFS driver implementation.

This structure needs to be defined before calling SDFatFS_init() and it must not be changed thereafter.

See also
SDFatFS_init()

Field Documentation

§ object

SDFatFS_Object* SDFatFS_Config::object

Pointer to a SDFatFS object


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale