Data Structures | Typedefs
AESGCMLPF3.h File Reference

Detailed Description

AESGCM driver implementation for the Low Power F3 family.

============================================================================

This file should only be included in the board file to fill the AESGCM_config struct.

Hardware Accelerator

The Low Power F3 family of devices has a dedicated AES hardware that can perform AES encryption operations with 128-bit keys. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted to ensure sensible access timeouts are set. The GHASH computation for GCM has optimizations using Shoup's 4-bit tables that are precomputed for each hash key H.

Implementation Limitations

Runtime Parameter Validation

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input parameter validation coverage is achieved by turning on assertions when compiling the driver.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESGCM.h>
#include <ti/drivers/cryptoutils/aes/AESCommonLPF3.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/aes.h)>
Include dependency graph for AESGCMLPF3.h:

Go to the source code of this file.

Data Structures

struct  AESGCMLPF3_Object
 AESGCMLPF3 Object. More...
 

Typedefs

typedef AESCommonLPF3_HWAttrs AESGCMLPF3_HWAttrs
 AESCCMLPF3 Hardware Attributes. More...
 

Typedef Documentation

§ AESGCMLPF3_HWAttrs

AESCCMLPF3 Hardware Attributes.

AESCCMLPF3 hardware attributes should be included in the board file and pointed to by the AESCCM_config struct.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale