Data Fields
ECDSALPF3SW_HWAttrs Struct Reference

ECDSALPF3SW Hardware Attributes. More...

#include <ECDSALPF3SW.h>

Data Fields

uint8_t dummy
 

Detailed Description

ECDSALPF3SW Hardware Attributes.

ECDSALPF3SW hardware attributes should be included in the board file and pointed to by the ECDSA_config struct.

Field Documentation

§ dummy

uint8_t ECDSALPF3SW_HWAttrs::dummy

The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale