ADC driver implementation for a MSP432 analog-to-digital converter.
============================================================================
Refer to ADCBuf.h for a complete description of APIs & example of use
|
#define | ADCBufMSP432_CMD_ENTER_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 1 |
| This control function enters ADC in low power mode. More...
|
|
#define | ADCBufMSP432_CMD_EXIT_ADC_ULTRA_LOW_POWER_MODE ADCBuf_CMD_RESERVED + 2 |
| This control function exits ADC from low power mode. More...
|
|
#define | ADCBufMSP432_P4_0_A13 ((13 << 10) | 0x0340) /* ch 13, port 4, pin 0 */ |
|
#define | ADCBufMSP432_P4_1_A12 ((12 << 10) | 0x0341) /* ch 12, port 4, pin 1 */ |
|
#define | ADCBufMSP432_P4_2_A11 ((11 << 10) | 0x0342) /* ch 11, port 4, pin 2 */ |
|
#define | ADCBufMSP432_P4_3_A10 ((10 << 10) | 0x0343) /* ch 10, port 4, pin 3 */ |
|
#define | ADCBufMSP432_P4_4_A9 ((9 << 10) | 0x0344) /* ch 9, port 4, pin 4 */ |
|
#define | ADCBufMSP432_P4_5_A8 ((8 << 10) | 0x0345) /* ch 8, port 4, pin 5 */ |
|
#define | ADCBufMSP432_P4_6_A7 ((7 << 10) | 0x0346) /* ch 7, port 4, pin 6 */ |
|
#define | ADCBufMSP432_P4_7_A6 ((6 << 10) | 0x0347) /* ch 6, port 4, pin 7 */ |
|
#define | ADCBufMSP432_P5_0_A5 ((5 << 10) | 0x0350) /* ch 5, port 5, pin 0 */ |
|
#define | ADCBufMSP432_P5_1_A4 ((4 << 10) | 0x0351) /* ch 4, port 5, pin 1 */ |
|
#define | ADCBufMSP432_P5_2_A3 ((3 << 10) | 0x0352) /* ch 3, port 5, pin 2 */ |
|
#define | ADCBufMSP432_P5_3_A2 ((2 << 10) | 0x0353) /* ch 2, port 5, pin 3 */ |
|
#define | ADCBufMSP432_P5_4_A1 ((1 << 10) | 0x0354) /* ch 1, port 5, pin 4 */ |
|
#define | ADCBufMSP432_P5_5_A0 ((0 << 10) | 0x0355) /* ch 0, port 5, pin 5 */ |
|
#define | ADCBufMSP432_P6_0_A15 ((15 << 10) | 0x0360) /* ch 15, port 6, pin 0 */ |
|
#define | ADCBufMSP432_P6_1_A14 ((14 << 10) | 0x0361) /* ch 14, port 6, pin 1 */ |
|
#define | ADCBufMSP432_P8_2_A23 ((23 << 10) | 0x0382) /* ch 23, port 8, pin 2 */ |
|
#define | ADCBufMSP432_P8_3_A22 ((22 << 10) | 0x0383) /* ch 22, port 8, pin 3 */ |
|
#define | ADCBufMSP432_P8_4_A21 ((21 << 10) | 0x0384) /* ch 21, port 8, pin 4 */ |
|
#define | ADCBufMSP432_P8_5_A20 ((20 << 10) | 0x0385) /* ch 20, port 8, pin 5 */ |
|
#define | ADCBufMSP432_P8_6_A19 ((19 << 10) | 0x0386) /* ch 19, port 8, pin 6 */ |
|
#define | ADCBufMSP432_P8_7_A18 ((18 << 10) | 0x0387) /* ch 18, port 8, pin 7 */ |
|
#define | ADCBufMSP432_P9_0_A17 ((17 << 10) | 0x0390) /* ch 17, port 9, pin 0 */ |
|
#define | ADCBufMSP432_P9_1_A16 ((16 << 10) | 0x0391) /* ch 16, port 9, pin 1 */ |
|
#define | ADCBufMSP432_PIN_NONE 0 |
|
#define | ADCBufMSP432_INTERNAL_SOURCE_PIN 0 |
|
|
enum | ADCBufMSP432_ReferenceSource { ADCBufMSP432_VREFPOS_AVCC_VREFNEG_VSS = ADC_VREFPOS_AVCC_VREFNEG_VSS,
ADCBufMSP432_VREFPOS_INTBUF_VREFNEG_VSS = ADC_VREFPOS_INTBUF_VREFNEG_VSS,
ADCBufMSP432_VREFPOS_EXTPOS_VREFNEG_EXTNEG = ADC_VREFPOS_EXTPOS_VREFNEG_EXTNEG,
ADCBufMSP432_VREFPOS_EXTBUF_VREFNEG_EXTNEG = ADC_VREFPOS_EXTBUF_VREFNEG_EXTNEG
} |
| ADCMSP432 reference source These fields are used by ADCBufMSP432_HWAttrs to specify the reference voltage for each channel. More...
|
|
enum | ADCBufMSP432_SamplingDuration {
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_4 = ADC_PULSE_WIDTH_4,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_8 = ADC_PULSE_WIDTH_8,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_16 = ADC_PULSE_WIDTH_16,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_32 = ADC_PULSE_WIDTH_32,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_64 = ADC_PULSE_WIDTH_64,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_96 = ADC_PULSE_WIDTH_96,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_128 = ADC_PULSE_WIDTH_128,
ADCBufMSP432_SamplingDuration_PULSE_WIDTH_192 = ADC_PULSE_WIDTH_192
} |
| ADCMSP432 sampling duration These fields define the MSP432 ADC sampling duration (sample and hold time) in the pulse width unit. User can specify the different sampling duration in the ADCBufMSP432_ParamsExtension when opening the ADC. More...
|
|
enum | ADCBufMSP432_TimerReferenceSource {
ADCBufMSP432_TIMERA0_CAPTURECOMPARE1 = 0,
ADCBufMSP432_TIMERA0_CAPTURECOMPARE2 = 1,
ADCBufMSP432_TIMERA1_CAPTURECOMPARE1 = 2,
ADCBufMSP432_TIMERA1_CAPTURECOMPARE2 = 3,
ADCBufMSP432_TIMERA2_CAPTURECOMPARE1 = 4,
ADCBufMSP432_TIMERA2_CAPTURECOMPARE2 = 5,
ADCBufMSP432_TIMERA3_CAPTURECOMPARE1 = 6
} |
| ADCMSP432 timer trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the Timer Capture for each channel. More...
|
|
enum | ADCBufMSP432_ClockSource {
ADCBufMSP432_ADC_CLOCK = ADC_CLOCKSOURCE_ADCOSC,
ADCBufMSP432_SYSOSC_CLOCK = ADC_CLOCKSOURCE_SYSOSC,
ADCBufMSP432_ACLK_CLOCK = ADC_CLOCKSOURCE_ACLK,
ADCBufMSP432_MCLK_CLOCK = ADC_CLOCKSOURCE_MCLK,
ADCBufMSP432_SMCLK_CLOCK = ADC_CLOCKSOURCE_SMCLK,
ADCBufMSP432_HSMCLK_CLOCK = ADC_CLOCKSOURCE_HSMCLK
} |
| ADCMSP432 clock source These fields are used by ADCBufMSP432_HWAttrs to specify the clock source for the ADC module. More...
|
|
enum | ADCBufMSP432_TriggerSource { ADCBufMSP432_TIMER_TRIGGER = ADC_MANUAL_ITERATION,
ADCBufMSP432_SOFTWARE_AUTOMATIC_TRIGGER = ADC_AUTOMATIC_ITERATION
} |
| ADCMSP432 trigger source These fields are used by ADCBufMSP432_HWAttrs to specify the trigger source for the ADC. More...
|
|
enum | ADCBufMSP432_DifferentialMode { ADCBufMSP432_SINGLE_ENDED = ADC_NONDIFFERENTIAL_INPUTS,
ADCBufMSP432_DIFFERENTIAL = ADC_DIFFERENTIAL_INPUTS
} |
| ADCMSP432 Differential Mode These fields are used by ADCBufMSP432_HWAttrs to specify if ADC differential sampling mode is selected. More...
|
|
enum | ADCBufMSP432_InternalSourceMode { ADCBufMSP432_INTERNAL_SOURCE_MODE_OFF = 0,
ADCBufMSP432_TEMPERATURE_MODE = ADC_TEMPSENSEMAP,
ADCBufMSP432_BATTERY_MONITOR_MODE = ADC_BATTMAP
} |
| ADCMSP432 Internal Source Mode These fields are used by ADCBufMSP432_HWAttrs to specify if a internal source mode is selected, i.e. temperature sensor or battery monitor modes. More...
|
|