48 #undef ChipInfo_GetSupportedProtocol_BV
49 #define ChipInfo_GetSupportedProtocol_BV NOROM_ChipInfo_GetSupportedProtocol_BV
50 #undef ChipInfo_GetPackageType
51 #define ChipInfo_GetPackageType NOROM_ChipInfo_GetPackageType
52 #undef ChipInfo_GetChipType
53 #define ChipInfo_GetChipType NOROM_ChipInfo_GetChipType
54 #undef ChipInfo_GetChipFamily
55 #define ChipInfo_GetChipFamily NOROM_ChipInfo_GetChipFamily
56 #undef ChipInfo_GetHwRevision
57 #define ChipInfo_GetHwRevision NOROM_ChipInfo_GetHwRevision
58 #undef ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated
59 #define ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated NOROM_ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated
111 if ( waferId == 0xB99A ) {
141 switch ( fcfg1Protocol ) {
151 if ( fcfg1UserId & ( 1 << 23 )) {
157 if ( fcfg1UserId & ( 1 << 24 )) {
187 switch ( fcfg1Rev ) {
203 switch ( fcfg1Rev ) {
214 switch ( fcfg1Rev ) {
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
static bool ChipInfo_HwRevisionIs_GTEQ_2_2(void)
Returns true if HW revision for this chip is 2.2 or greater.
HwRevision_t
HW revision enumeration.
PackageType_t
Package type enumeration.
-1 means that the chip's family member is unknown.
-1 means that current chip type is unknown.
4 means that this is a WCSP chip (flip chip).
21 means that the chip's HW revision is 2.1
ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV(void)
Returns bit vector showing supported protocols.
static uint32_t ChipInfo_GetUserId(void)
Returns the 32 bits USER_ID field.
void ThisCodeIsBuiltForCC26xxHwRev22AndLater_HaltIfViolated(void)
Verifies that current chip is built for CC26xx HwRev 2.2 or later and never returns if violated...
5 means that this is a CC2650 chip.
-1 means that the chip type is unknown.
7 means that this is a CUSTOM_1 chip.
3 means that this is a CC2630 chip.
6 means that this is a CUSTOM_0 chip.
-1 means that the chip's HW revision is unknown.
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
20 means that the chip's HW revision is 2.0
4 means that this is a CC2640 chip.
22 means that the chip's HW revision is 2.2
ChipType_t
Chip type enumeration.
ChipFamily_t
Chip family enumeration.
static bool ChipInfo_ChipFamilyIsCC26xx(void)
Returns true if this chip is member of the CC26xx family.
ProtocolBitVector_t
Enumeration identifying the protocols supported.
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
1 means that the chip is a CC13x0 family member.
static uint32_t ChipInfo_GetDeviceIdHwRevCode(void)
Returns the internal chip HW revision code.
ChipType_t ChipInfo_GetChipType(void)
Returns chip type.
2 means that the chip is a CC26x1 family member.
10 means that the chip's HW revision is 1.0
2 means that this is a CC2620 chip.
0 means that this is a 4x4mm chip.
static uint32_t ChipInfo_GetMinorHwRev(void)
Returns minor hardware revision number.
3 means that the chip is a CCxxx2/xxx4 family member.
4 means that the chip is a CC26x0_R2 family (new ROM contents).
0 means that the chip is a CC26x0 family member.