#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_adi.h>
#include <inc/hw_adi_2_refsys.h>
#include <inc/hw_adi_3_refsys.h>
#include <inc/hw_aon_ioc.h>
#include <inc/hw_aon_sysctl.h>
#include <inc/hw_aon_wuc.h>
#include <inc/hw_aux_wuc.h>
#include <inc/hw_ccfg.h>
#include <inc/hw_fcfg1.h>
#include <inc/hw_flash.h>
#include <inc/hw_prcm.h>
#include <inc/hw_vims.h>
#include <driverlib/aon_wuc.h>
#include <driverlib/aux_wuc.h>
#include <driverlib/chipinfo.h>
#include <driverlib/setup.h>
#include <driverlib/setup_rom.h>
Go to the source code of this file.
Macros | |
#define | CPU_DELAY_MICRO_SECONDS(x) CPUdelay(((uint32_t)((( x ) * 48.0 ) / 5.0 )) - 1 ) |
Functions | |
static void | TrimAfterColdReset (void) |
Trims to be applied when coming from PIN_RESET. More... | |
static void | TrimAfterColdResetWakeupFromShutDown (uint32_t ui32Fcfg1Revision) |
Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET). More... | |
static void | TrimAfterColdResetWakeupFromShutDownWakeupFromPowerDown (void) |
Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET). More... | |
void | SetupTrimDevice (void) |
Performs the necessary trim of the device which is not done in boot code. More... | |
#define CPU_DELAY_MICRO_SECONDS | ( | x | ) | CPUdelay(((uint32_t)((( x ) * 48.0 ) / 5.0 )) - 1 ) |
|
static |
Trims to be applied when coming from PIN_RESET.
Definition at line 389 of file setup.c.
Referenced by SetupTrimDevice().
|
static |
Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET).
Definition at line 269 of file setup.c.
Referenced by SetupTrimDevice().
|
static |
Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET).
Definition at line 253 of file setup.c.
Referenced by SetupTrimDevice().