CC13xx Driver Library
aon_wuc.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_ints.h"
#include "../inc/hw_aon_wuc.h"
#include "../inc/hw_aon_rtc.h"
#include "interrupt.h"
#include "debug.h"

Macros

#define AONWUC_CLOCK_SRC_HF   0x00000003
 
#define AONWUC_CLOCK_SRC_LF   0x00000001
 
#define AONWUC_NO_CLOCK   0x00000000
 
#define AUX_CLOCK_DIV_2   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV2 )
 
#define AUX_CLOCK_DIV_4   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV4 )
 
#define AUX_CLOCK_DIV_8   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV8 )
 
#define AUX_CLOCK_DIV_16   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV16 )
 
#define AUX_CLOCK_DIV_32   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV32 )
 
#define AUX_CLOCK_DIV_64   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV64 )
 
#define AUX_CLOCK_DIV_128   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV128 )
 
#define AUX_CLOCK_DIV_256   ( AON_WUC_AUXCLK_SCLK_HF_DIV_DIV256 )
 
#define AUX_CLOCK_DIV_UNUSED   ( AON_WUC_AUXCLK_SCLK_HF_DIV_M + ( 1 << AON_WUC_AUXCLK_SCLK_HF_DIV_S ))
 
#define AUX_CLOCK_DIV_M   ( AON_WUC_AUXCLK_SCLK_HF_DIV_M )
 
#define MCU_VIRT_PWOFF_DISABLE   0x00000000
 
#define MCU_VIRT_PWOFF_ENABLE   0x00020000
 
#define MCU_IMM_WAKE_UP   0x00000000
 
#define MCU_FIXED_WAKE_UP   0x00010000
 
#define AUX_VIRT_PWOFF_DISABLE   0x00000000
 
#define AUX_VIRT_PWOFF_ENABLE   0x00020000
 
#define AUX_IMM_WAKE_UP   0x00000000
 
#define AUX_FIXED_WAKE_UP   0x00010000
 
#define MCU_RAM0_RETENTION   0x00000001
 
#define MCU_RAM1_RETENTION   0x00000002
 
#define MCU_RAM2_RETENTION   0x00000004
 
#define MCU_RAM3_RETENTION   0x00000008
 
#define MCU_RAM_BLOCK_RETENTION   0x0000000F
 
#define MCU_AUX_RET_ENABLE   0x00000001
 
#define AONWUC_AUX_WAKEUP   0x00000001
 
#define AONWUC_AUX_ALLOW_SLEEP   0x00000000
 
#define AONWUC_OSC_GBIAS_REQ   0x00400000
 
#define AONWUC_AUX_GBIAS_REQ   0x00200000
 
#define AONWUC_MCU_GBIAS_REQ   0x00100000
 
#define AONWUC_OSC_BGAP_REQ   0x00040000
 
#define AONWUC_AUX_BGAP_REQ   0x00020000
 
#define AONWUC_MCU_BGAP_REQ   0x00010000
 
#define AONWUC_GBIAS_ON   0x00002000
 
#define AONWUC_BGAP_ON   0x00001000
 
#define AONWUC_AUX_POWER_DOWN   0x00000200
 
#define AONWUC_MCU_POWER_DOWN   0x00000100
 
#define AONWUC_JTAG_POWER_ON   0x00000040
 
#define AONWUC_AUX_POWER_ON   0x00000020
 
#define AONWUC_MCU_POWER_ON   0x00000010
 
#define AONWUC_SPLY_POWER_DOWN   0x00000001
 
#define MCU_RAMREPAIR_DONE   0x00000001
 
#define AUX_RAMREPAIR_DONE   0x00000002
 
#define RC_RATE_MAX   768
 
#define RC_RATE_MIN   2
 
#define AONWUC_MCU_RESET_SRC   0x00000002
 
#define AONWUC_MCU_WARM_RESET   0x00000001
 

Functions

static void AONWUCMcuPowerDownConfig (uint32_t ui32ClkSrc)
 Configure the power down clock for the MCU domain. More...
 
static void AONWUCMcuPowerOffConfig (uint32_t ui32Mode)
 Configure the power down mode for the MCU domain. More...
 
static void AONWUCMcuWakeUpConfig (uint32_t ui32WakeUp)
 Configure the wake-up procedure for the MCU domain. More...
 
static void AONWUCMcuSRamConfig (uint32_t ui32Retention)
 Configure the retention on the block RAM in the MCU domain. More...
 
static uint32_t AONWUCAuxClockConfigGet (void)
 Return the clock configuration for the AUX domain. More...
 
static void AONWUCAuxPowerDownConfig (uint32_t ui32ClkSrc)
 Configure the power down mode for the AUX domain. More...
 
static void AONWUCAuxSRamConfig (uint32_t ui32Retention)
 Configure the retention on the AUX SRAM. More...
 
static void AONWUCAuxWakeupEvent (uint32_t ui32Mode)
 Control the wake up procedure of the AUX domain. More...
 
void AONWUCAuxReset (void)
 Reset the AUX domain. More...
 
static void AONWUCAuxImageValid (void)
 Tells the Sensor Controller that the image in memory is valid. More...
 
static void AONWUCAuxImageInvalid (void)
 Tells the Sensor Controller that the image in memory is invalid. More...
 
static uint32_t AONWUCPowerStatusGet (void)
 Get the power status of the device. More...
 
static void AONWUCShutDownEnable (void)
 Enable shut-down of the device. More...
 
static void AONWUCDomainPowerDownEnable (void)
 Enable power down mode on AUX and MCU domain. More...
 
static void AONWUCDomainPowerDownDisable (void)
 Use this function to disable power down mode of the MCU and AUX domain. More...
 
static void AONWUCMcuResetClear (uint32_t ui32Status)
 Use this function to clear specific status bits. More...
 
static uint32_t AONWUCMcuResetStatusGet (void)
 Return the reset status. More...
 
void AONWUCRechargeCtrlConfigSet (bool bAdaptEnable, uint32_t ui32AdaptRate, uint32_t ui32Period, uint32_t ui32MaxPeriod)
 Configure the recharge controller. More...
 
static uint32_t AONWUCRechargeCtrlConfigGet (void)
 Get the current configuration of the recharge controller. More...
 
void AONWUCOscConfig (uint32_t ui32Period)
 Configure the interval for oscillator amplitude calibration. More...
 
static void AONWUCJtagPowerOff (void)
 Request power off of the JTAG domain. More...